AXIS#.WS.FREQ

Description

This keyword sets the excitation frequency for Wake and Shake mode 2.

The default setting of 10Hz will work for almost all systems.

In cases where the load attached to the motor is much higher than the motor inertia (200:1) it may be necessary to lower the value of AXIS#.WS.FREQ.

Effects of lowering AXIS#.WS.FREQ:

  • Wake and Shake Mode 2 will take longer to complete.
  • A higher magnitude of motion will be seen on the motor because the motor has current applied in the same direction for a longer period of time.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Hz

Range

0.01 - 8000

Default Value

10

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Related Topics

AXIS#.WS.MODE

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen